Prysmian to launch VerTV™, the new optimized system for use in Satellite TV via
fibre cabling
Prysmian launched the new VerTV™ system for Satellite TV via fibre at
"Impronta Digitale - National Edition", a major event organized by Sky Italia in Rome.
Satellite TV, which has traditionally used coaxial/copper cable for the final customer
connection, is gradually migrating towards the use of fibre optic technology, driven by the ever
growing demand for new high bandwidth services offered within the market. The transmission capacity
of fibre is basically unlimited, and due to their high strength, small size and extreme
flexibility, fibre optic cables can be easily installed in the reduced spaces often present in the
domestic housing environment.
Sky has recognised the advantages of optical technology and is one of the early
adopters of the technology within the Satellite TV world.
In response to this need Prysmian has undertaken an extensive programme of product
development aimed at producing an
optimized system for fibre TV cabling and has become one of Sky's
official technological partners in its migration towards fibre. The
VerTV™ system is the result of this work and is a testimony to Prysmian's
experience in optical fibres, cables and systems. Designed to be compatible with every Multi
Dwelling Unit TV cabling requirement, it consists of
pre-connectorised patchcords, floor boxes and a dedicated mini-connector which,
thanks to its reduced dimensions, allows easy installation within existing ducts. All parts of the
system have been designed in line with the strictest environmental requirements including full
compliance with all safety and fire regulations for indoor cabling. The system has been designed
with ease and efficiency of installation being key criteria. No splices - fusion nor mechanical -
are required in the field due to the pre-connectorised approach. It is
fast and simple to install and with the number of components kept to a minimum
there is no need for the installer to maintain high stock levels of specific items.
VerTV™ represents another important milestone for Prysmian in its ongoing commitment to
providing its customers with the latest and best product innovation in today's rapidly evolving
broadband society. For full details on all of Prysmian's product portfolio go to www.prysmian.com
Related information
VerTV™ - Sistema in Fibra Ottica
per TV SAT
Highlights
Archive
|