RSS  |  Glossary  |  Contacts |  Italiano  |  Search

  
One Company
About us
Solutions for your business
Investor Relations
People & Careers
Media & Communication
Home    Solutions for your business: Fire Safety    Topics of interest
Our business
Fire Safety
Fire resistant cables
Low Fire-Hazard Cables
Topics of interest
Applications and References
Escape Simulation
News
Downloads
Events
Highlights Archive

Topics of Interest

Prysmian is investing in Safety and decided to organize this site to enable the diffusion of scientific knowledge to all Electricity Professionals, Opinion Leaders, Authorities and End-Users so they can be updated and act with coherence in the European Common Market.
This part of the site is intended to provide a coherent framework to evaluate the contribution of cables to safety during fire:

  starting form the physiological effects of smoke and gases which are the real threat in case of fire
  confirming that it is possible to evaluate the threat generated by combustion products through modern techniques (FTIR) for measuring the composition of the gases cocktail (quantity and quality) of the effluent during the development of a fire
  revealing that the acidity parameter present in the Euroclassification of cables was shown to be a good predictor of irritant effects when compared with the FEC index calculated from effluents measured as above
  showing the threats in case of fire by simulating with modern computing the diffusion of combustion products in a building and the behavior of occupants in case of a fire alarm
  finally illustrating the route to CE marking under the CPD 

 Hazard of combustion
The target of this paper is to provide scientific bases to the statement (manifest, but generic) that the main cause of injury and death in fires is incapacitation resulting from exposure to fire effluent (smoke and gases). During fires, physiological effects dominate and determine time to incapacitation. The sequence of physiological hazards in developing fires can be applied to fire safety engineering design of buildings and to the evaluation of products for use in them using appropriate calculation methods for assessment of time to incapacitation. (Courtesy Europacable) 
Physiological effects of combustion products and fire hazard assessment by Professor David A. Purser (323 KB)

Smoke and Acidity
A threat in case of fire is the quality of combustion product; an evaluation of the threat generated is possible if the composition of the gases cocktail (quantity and quality) of the effluent during the development of the fire is known. The FTIR technique used in this project has given high reliability in detection of combustion gases and can be conveniently used with the prEN50399 fire scenario to fully investigate the reaction to fire of cables. (Courtesy Europacable) 
Feasibility study of supplementary FTIR measurements in Tests with electric cables according to Commission by Björn Sundström (210 KB)
The acidity parameter has been used for many years by the cable industry to indicate the corrosive potential of effluents from burning cables. This research revealed that this parameter was shown to be a good predictor of irritant effects compared with the FEC index calculated from effluent measurements by FTIR. (Courtesy Europacable) 
Investigation into the smoke effluents of burning cables” by Silvio Messa (199 KB)

Escape Simulation
Other studies have clarified that gases and smoke are the real threat in case of fire, that it is possible to measure cable fire emissions with modern techniques (FTIR), that acidity is a good predictor of irritant effects of cable emissions. It is now necessary to investigate the correlation between these parameters and cable applications. Thanks to modern computing it is possible to measure the threats in case of fire by simulating the diffusion of combustion products in a building and the behavior of occupants in case of a fire alarm. The University of Lund conducted a study using input data from the measurement of components of combustion made using the prEN50399 fire test scenario and found that the adoption of non halogenated cables could significantly reduce the fire hazard. (Courtesy Europacable) 
Simulation of critical evacuation conditions for a fire scenario involving cables and comparison of two different cables” by Patrick van Hees and Daniel Nilsson (499 KB)

Construction Products Directive 
The objective of this series of papers is to illustrate the route to CE marking under the CPD and to explain some of the actions that have to be carried out before this marking can be achieved.
Reaction to fire classification for cables  (137 KB)
Standards required to support CE marking of cables  (112 KB)
The CEMAC II project  (89 KB)
A simplified certification process for CE marking of cables under the CPD  (86 KB)
Site Map  |  Legal Information  |  Company info  |  Copyright © 2012 All rights reserved. Last Revised Date: May 21, 2010