The aurora borealis — as this event is scientifically defined — is one of the effects of geomagnetic storms, a cosmic phenomenon that has the potential to significantly impact our daily lives. Geomagnetic storms, one of the most fascinating and potentially disruptive events that can take place in the vast expanse of space, are caused by disturbance in the Earth’s magnetic field. More specifically, they originate from the sun, where powerful bursts of energy and charged particles are expelled during solar flares or coronal mass ejections (CMEs). When these particles interact with the Earth's magnetosphere, they can cause disturbances in the magnetic field, leading to a geomagnetic storm. While the Earth's magnetic field acts as a shield, protecting us from the majority of solar radiation, intense storms can still penetrate this barrier and impact the planet in several ways.
This phenomenon can in fact have a wide range of effects, from stunning auroras to potentially damaging disruptions of our technological systems.