Prysmian: Battaini, “Geopolitics and Electrification Are Reinforcing Our Local-for-Local Model. We Do Not See an AI Bubble”

press-note-banner

Prysmian: Battaini, “Geopolitics and Electrification Are Reinforcing Our Local-for-Local Model. We Do Not See an AI Bubble”


“The geopolitical landscape is extremely dynamic, and it rewards the agility of a group like Prysmian, which over the years has been able to anticipate change and seize new opportunities. We have invested around €9 billion in acquisitions in the United States because we had identified significant growth potential in the US market and structurally stronger demand,” said Massimo Battaini, Prysmian CEO, speaking today at the Affari & Finanza main event at SDA Bocconi in Milan.

 

Battaini: “Our model has always been local for local: producing locally to serve local markets and communities. We do not operate according to a global supply chain logic. The current geopolitical landscape has reinforced this strategy and, at the same time, is accelerating the need for greater energy independence in Europe. Renewables are fundamental to this transition, and Prysmian plays a leading role in the energy transition, connecting renewable generation, often geographically distant, to the places where energy is actually used.”

 

Battaini: “Europe and the United States are fundamentally different. The United States is a single market, including when it comes to the infrastructure needed to distribute energy and data, while Europe remains much more fragmented. The US market also benefits from a strong push towards local production.”

 

“We do not currently see signs of a potential AI bubble. On the contrary, demand continues to grow. Compared with the first half of the year, which was already up on last year, in the third and fourth quarters we recorded a further increase in demand for power and optical cables. Hyperscalers continue to ask us for large volumes of cables because they have billions in investments currently being deployed,” Battaini said. “The fiber market has also faced a shortage of production capacity, initially driven not by AI but by rising demand linked in part to military applications, particularly the use of fiber to control drones. AI is now adding further pressure to demand that was already very strong.”

 

“At the same time, the growth of data centers raises a fundamental issue: their sustainability and their impact on communities, starting with energy and water consumption. The way forward is to produce more renewable energy and make it available where data centers are located, while also innovating the infrastructure that connects them,” Battaini continued. “This is exactly where innovation can make a difference. We have developed hollow-core fiber, in which the signal travels through air, enabling faster transmission and allowing the distance between infrastructure sites to be significantly increased. This can help locate data centers farther away from major consumption centers, reducing pressure on grids and local communities. At the same time, we supply some data centers with low carbon aluminum cables. We believe innovation is the way to make the growth of data centers sustainable without limiting their development.”

 

Battaini: “Submarine infrastructure has also become a strategic asset. Cables are protected using burial systems adapted to the different characteristics of the seabed. We have developed specific technologies and tools, such as large ploughs towed by our vessels, which allow us to lay and protect cables. Submarine power systems also integrate optical fiber, enabling us to monitor the infrastructure and intervene quickly when needed. In Palermo, we are developing solutions capable of monitoring parameters such as power quality, temperature and acoustics. The digitalization of infrastructure therefore allows us not only to transmit energy, but also to understand in real time how these assets are performing.”

 

Battaini: “Another key challenge for electrification concerns raw materials. Copper is an increasingly strategic resource, and demand is set to grow. Here too, innovation is essential to address scarcity by using resources more efficiently and developing solutions to recover and recycle copper.”

 

Battaini: “We operate in a market that is changing at extraordinary speed. That is why, above all, I would tell young people to remain curious, versatile and determined. At Prysmian, we talk a lot about tenacity: it means being able to adapt without losing sight of the goal. It is a mindset we have applied many times throughout our history, and one that will remain fundamental as we navigate the transformations ahead.”