Prysmian Group’s Leonardo da Vinci cables installation vessel wants YOU!
We at Prysmian Group put all our energy and expertise into designing and delivering the most advanced and eco-friendly submarine cable installation ship yet: the Leonardo da Vinci, which was delivered in August. We are thrilled that the people at Offshore Wind Journal have shortlisted it for the “Best Support Vessel of the Year” at the upcoming Gala Dinner on November 17. The Leonardo da Vinci is the best candidate for the award because of its industry-leading features. We made it hybrid-battery-powered to comply with the most stringent international requirements. The high cable load capacity and navigation speed of over 16 knots mean the Leonardo da Vinci can reduce the number of cable installation campaigns of any project, saving time and money. It can reach cable laying depths of 3,000 meters, and its two carousels of 7,000 and 10,000 tonnes are the highest load capacity in the market. We hope you agree that Leonardo da Vinci is leading the way, and if you do, please vote for us by October 20! You can cast your vote here: Annual OSJ conference awards.