The invention of the Internet
Thanks to the scale of the digital revolution, for most of us, trying to imagine our lives today without the Internet is an impossibility. In simple terms, the Internet is a global network of computers that communicate in a standardized way, like a network of networks that aims to allow any device to communicate with any other device.
The invention of the Internet led to the greatest expansion of information access in human history, facilitating a spread of knowledge that was inconceivable even as recently as the early 1990s.
Worldwide Internet users are currently estimated at more than 5 billion, roughly 63% of the global population. That ever-increasing trend also saw a surge in its growth rate during the COVID-19 pandemic. But who was responsible for this huge jump in human development and when did it take place?