press -transmission

Prysmian successfully completes Gruissan/EOLMED floating offshore wind farm export cable in France

categories:

Strong commitment to project execution in support of the decarbonisation

Milan, Italy   -   May 30, 2024 - 10:00 AM

Prysmian, world leader in the energy and telecom cable systems industry, announces the successful completion of the Gruissan/EOLMED floating offshore wind farm project in France. Prysmian had secured this project in 2021 with a contract signed with the French TSO RTE (Réseau de Transport d'Électricité) for the Engineering, Procurement, Construction and Installation (EPCI) of an export submarine power cable system.

Prysmian was responsible for the design, supply, installation, termination, testing, and commissioning of a 66 kV static three-core export submarine cable with EPR insulation for a total of 23 km and a 66 kV dynamic submarine export tail with EPR insulation connecting the onshore grid to the floating electrical hub of EOLMED’s 30MW offshore floating wind farm (currently under construction).

With this high-profile engineering project and 2nd EPCI turnkey project for dynamic cable systems, Prysmian has further consolidated its position in the floating offshore wind farm market, deploying its knowledge, experience, and capability to provide innovative dynamic cable systems solutions that allow to build offshore wind farms in deeper water areas.

“With this project, which follows Provence Grand Large (PGL) floating offshore wind farm, Prysmian demonstrates once again its leading position in the market and the validity of its know-how and technologies in the development of submarine cables and systems to support smarter and greener power grids worldwide” commented Alberto Boffelli, COO Transmission, Prysmian.

download file