1150x650_LayoutPressRelease_Transmission.jpg

PRYSMIAN TO BOOST ENERGY SECURITY IN NEW ZEALAND

categories:

CAPACITY RESERVATION AGREEMENT WITH TRANSPOWER NEW ZEALAND LTD TO RESERVE CAPABILITY TO DELIVER A SUBMARINE POWER INTERCONNECTOR PROJECT

Milan, Italy   -   13/12/2024 - 08:30 AM

Prysmian has signed a capacity reservation agreement of around €250 million with Transpower New Zealand Ltd, the New Zealand TSO, for a new submarine power cables across Cook Strait, connecting Aotearoa New Zealand’s North and South Islands. With an overall capacity of up to 1400 MW, the new power link will replace existing cable infrastructure which is nearing the end of its operational life, providing significant benefits to the country, ensuring reliable and cost-effective electricity supply, while supporting the increasing electricity demand in New Zealand. 

New Zealand, which has no power connections with other countries, relies on its inter- island submarine power cables to move power from established renewable hydro generation in the South Island to growing population centres in the North Island across the 40km wide Cook Strait. Two-way power flow through the link is critical to ensure that in ‘dry years’, where rainfall and snowmelt does not provide sufficient storage into hydro schemes, bulk power can be transferred in the opposite direction (North Island to South Island), as was seen in 2024. 

Prysmian will make available a full turnkey solution for the project, also with its state- of-the-art and proprietary EOSS monitoring system in place. An essential service that will help ensure the long-term security and lifespan of the project. 

The contract will now be negotiated and is expected to be finalised in Q1 2026 with a notice to proceed expected by 1H 2026, and commissioning planned in 2031. 

 

THE TECHNICAL DETAILS 

Prysmian has reserved the capacity to design, test, supply and install a HVDC (High Voltage Direct Current) Cable System, consisting of 350 kV single-core cables with MI (Mass Impregnated) insulation and double-wire armouring and integrated fiber optic – essential for monitoring purposes. 

The capacity to manufacture submarine cable has been reserved at Prysmian’s centre of excellence in Arco Felice (Italy), while the capacity for the installation operations has been reserved with one of the new Company’s record-setting cable-laying vessels (like Monna Lisa class), due to the water depth of around 250 meters. 

 

FULLY INTEGRATED SOLUTION USING PRYSMIAN’S PROPRIETARY TECHNOLOGY 

Prysmian will also make use of its proprietary fully integrated EOSS monitoring system based on more than 20 years’ experience in this field. All cables will be constantly monitored using the EOSS innovative solutions like Distributed Temperature (DTS) and Acoustic Sensing (DAS) to measure all key operating parameters along with the whole cable system. As a turnkey solution provider, Prysmian can offer its comprehensive 360° strategic approach by integrating innovative and smart components with consolidated cable technologies, leveraging on the widest range of installation capabilities.

 

download file