Prysmian end-of-life statement

The final phase of a product life cycle is called End Of Life (EOL): in this stage a product is no more able to fulfill the task/function for which it has been designed and therefore is going to be disposed.

Prysmian’s commitment in terms of end-of-life responsibility is clearly demonstrated by its breakthrough P-Laser technology, which the Company has been pioneering and developing since early 2000s. Indeed, this technology — which uses fully thermoplastic materials as power cable insulation — offers the most attractive advantages in the end-of-life phase of the product lifecycle, as it is possible to recycle 100% of the materials composing the cable, including its plastic layers.

In addition, this technology ensures an efficient manufacturing process, characterised by lower power consumption and energy savings. The absence of any degassing treatments avoids emissions in the atmosphere, with a lower environmental impact for the whole process. Moreover, the production of MV power cables requires a compact manufacturing site, with lower soil occupation. However, the most valuable feature of this technology is full recyclability of polymeric materials, with benefits in terms of carbon footprint.

 

Unlike cables with XLPE insulation — the insulation materials most widely used in today’s cable industry —, this technology offers the possibility of fully recycling the cable’s materials.

Today, the use of the P-Laser technology is well-established for MV cables, with more than 90,000 km of cables installed in Italy and The Netherlands. In addition, this technology has been validated for application in HVAC cables and is qualified for the highest insulation levels of HVDC systems, up to 600 kV, with 1,200 km produced. Indeed, this technology was selected for the biggest HVDC land project ever (German Corridors), for which about half of the cable length is being produced in the P-Laser version.

In addition, development works are underway to extend the P-Laser technology also to LV cables, so as to apply the thermoplastic insulation technology to the entire power cable range

 

 

At the end of 2024, Prysmian’s product portfolio included for 86.7%* materials characterized by potential end-of-life recyclability. The remainder consisted of materials that cannot be reintroduced in the production cycle and are ultimately meant for disposal (landfill or incinerator).

 

*excluding the contribution of Encore Wire acquisition for which the information is not yet fully integrated for the scope of this KPI calculation

DESIGN TO COST

Another practical example of Prysmian’s commitment to the end-of-life responsibility is the Design To Cost programme.

It consists of a holistic approach based on a lower TCO (total cost of ownership) of materials and a comprehensive process that takes into account design, standards/specifications, materials, ingredients, cable processes/routing, compounding, and external competitors benchmarking. This activity, together with the ongoing rationalisation of product families, represents a methodology to lower production costs, both when developing a new product and when reengineering an existing one, using the best materials, adopting efficient processes and implementing innovative projects. Moreover, the design optimisation leads to a reduction in the volumes to be transported and distributed, thus allowing to cut the environmental impact and significantly reduce the effects even on the logistic side.

This activity provides a relevant impact on the end of life of cable products, due to the significant reduction in the amounts of materials to be disposed of (wasted or possibly recycled) and the related activities/energy consumption associated to the cable disposal.

2024 was a record year for the DESIGN TO COST (DTC) programme, not only driven by the strong impetus generated by the significant growth in the Group’s revenues. The final result was 61.4 million. The DTC program helped mitigate variable cost inefficiencies (mainly attributable to raw material shortages and their price volatility) and improve the competitiveness of our products in several segments.

SUBSTANCES OF VERY HIGH CONCERN (SVHC)

In the context of an increasingly stringent legislation on the use of some particularly hazardous substances – so-called Substances of Very High Concern (SVHC) — and on substances subject to the ROHS Directive, Prysmian has defined and implemented actions focused on minimizing or phasing out said substances, with the aim to avoid both their processing in the supply chain and their presence in the final waste stream, when products are disposed of, making them more recyclable at their EOL phase, with overall positive implications for both the environment and product safety.

In this perspective, Prysmian is completing the implementation of an automatic system for tracking the possible presence of said substances in its final products, while also phasing them out in an increasing number of products, including substances whose use, though being SVHC, is not yet banned. In 2024, the revenues associated with products containing substances in this list amounted to a total of 10%-20% on the total revenues (standing in the lower end of this range) with a commitment to substitute them by 2028.

Prysmian’s Commitment to Replacing Hazardous Substances

Prysmian is committed to a proactive and responsible approach to chemical management, aligned with principles of sustainability and health protection, which are central to the company’s strategy. In particular, the company actively collaborates with leading industry associations such as Europacable and Cefic to identify and develop alternatives to hazardous substances. This commitment is also reflected in a direct allocation from the Group R&D team’s budget, specifically dedicated to projects aimed at replacing or phasing out substances classified as hazardous, including those on ECHA’s SVHC list.

 

Prysmian adopts a “timely and conservative” approach in the continuous update of its SVHC substance analysis, integrating this into its business processes. The substitution program is real and structured, with a target timeline set for 2028, with the exception of the replacement of metallic lead in submarine applications, where substitution is explicitly considered the most concrete and lasting lever for a safe transition to alternative materials.

Use Cases and Ongoing Projects

The lead-free solution for lead sheaths in extruded land cables has been developed and fully qualified up to the highest voltage classes (400 kV AC, 525 kV DC). In addition, R&D activities are underway for innovative solutions in submarine applications, based on hermetic barriers using alternative metals, fully polymeric materials, or hybrid configurations. However, the lack of recognized international standards remains a challenge for qualifying these solutions, slowing down the substitution and phase-out program.

A project is underway with the coating supplier to replace TPO with alternative substances. Various formulations are currently being evaluated, starting with the outermost layers of the optical fiber coating system, considered less critical.

Prysmian limits the use of PFAS to polymeric versions, which are considered less hazardous compared to small fluorinated molecules. Although valid alternative techniques are not yet available for certain applications (e.g., aerospace, defense, chemical resistance), the company is implementing a concrete elimination plan, where feasible, through the following main actions:

1. Removal of PFAS-based process additives;

2. Reduction of PFAS insulating materials in flame-retardant multimedia cables;

3. Implementation of a traceability system to identify and monitor the quantity and type of PFAS present in the cables.

A phase-out plan is underway for the use of MCCPs as plasticizers in PVC compounds, both in Europe and globally. To achieve these targets, evaluations are being conducted on both bio-based alternatives and transitions to longer-chain MCCPs (not included in the REACH Regulation).

The development of lead-free insulating compounds for cable insulation is at an advanced stage, with qualification expected to be completed by the end of 2025, extending to both submarine and land cables for medium and high voltage. The application is being extended to network components for MV and HV cables, which will enter a pre-qualification phase by the end of 2025.

Methodology of Simplified LCA (Carbon Footprint & Potential Recyclability)

Simplified LCA results of all cables can be calculated in Common Analisi – the design tool with construction information of all cables. These results are related to cradle to gate carbon footprint assessment and potential recyclability of the product’s materials at the end of life. To do that, this is the procedure followed:

1. Selection of relevant inventory data:

  • Airborne emissions of cables raw materials (per kg of material);
  • Airborne emissions of Prysmian plants electricity consumption (per kWh);

2. Assessment of said inventory data into CO2 equivalent values, in term of CO2eq emission factor per kg (for the material) and per kWh (for the electricity country mixes);

3. Flag the raw materials as potential recyclable or not recyclable;

4. Uploading of said relevant inventory data into Common Analisi tool, after having implemented in it a functionality to calculate the CO2eq per km of cable, that automatically multiplies;

  • the amount of cables materials by its CO2 eq emission factors (emissions related to all the materials used for the cable production);
  • the amount of kWh consumed for that cable by the electricity CO2eq emission factor (electrical energy related to all the production phases of the cable manufacturing process);

5. When queried a given cable, CA includes – in its construction report – the CO2 of said cable, split into Raw Materials contribution and Routing (Prysmian process) contribution;

6. Final calculation of cables materials potential recyclability.

Prysmian LCA approach

LCA in Prysmian are carried out on specific products upon request of “Environmental Product Declaration” by customers in the context of commercial tenders, or upon internal initiative to cover such products with EPD itself. As a matter of fact, LCA is the basis of EPD, therefore LCA activities of Prysmian are mainly aimed at obtaining certificated EPDs with some rare exceptions . In any case, LCA in Prysmian are developed looking at ISO 14040 standard and more specific standards regulating the EPD, specifically ISO 14025, EN 50693, EN 15804, PCR of Program Operators . Prysmian EPDs are then published on the site of such Program Operator releasing the specific rules to follow for cables EPD.