Battery Energy Storage Systems (BESS): Cable, Connectivity and Monitoring Solutions

Reliable BESS infrastructure for renewable energy storage, grid stability and long-term performance

 

Battery Energy Storage Systems (BESS) store electricity when renewable generation exceeds demand and release it when power is needed. By supporting grid balancing, peak shaving, backup power and the integration of solar and wind energy, BESS technologies are becoming essential to modern, resilient and low-carbon power networks.

Prysmian provides BESS cable solutions, accessories, monitoring technologies and services designed for utility-scale energy storage plants, commercial and industrial installations, renewable energy projects and grid connection infrastructure. Our portfolio helps developers, EPC contractors, utilities, system integrators and asset owners improve safety, simplify installation and protect long-term system reliability.

The Prysmian Advantage for BESS Projects

One-Stop Shop for BESS Connectivity

Complete connectivity from battery racks to grid connection

Prysmian delivers an integrated BESS connectivity ecosystem across the entire energy storage architecture, helping customers manage every critical connection point with one trusted partner. Our portfolio includes:

DC battery cables for high-power energy storage systems

Low Voltage AC and grounding cables

Medium and High Voltage power cables

Communications and MMS cables

Fibre optic cables for high-speed BESS communication and monitoring

Fire-protection and fire alarm cables

Control and instrumentation cables

Cable accessories and joints

Climate control and cooling

By providing complete BESS cable and connectivity solutions from battery racks to grid connection, Prysmian helps simplify project execution, reduce interface risk and ensure reliable performance across the full energy storage system.

 

BESS-Engineered Cable Performance

Fit-for-purpose cable solutions designed for battery energy storage applications

BESS installations place specific demands on electrical infrastructure. High current loads, compact layouts, challenging outdoor conditions and strict safety requirements call for cable systems engineered specifically for battery energy storage, not simply adapted from standard products.

Prysmian’s solutions address the technical and operational challenges of battery energy storage installations while supporting efficient energy transfer, safer operation and optimized performance throughout the asset lifecycle.

End-to-End Support for BESS Projects

From system design to installation, commissioning and long-term asset performance

Prysmian supports BESS projects beyond cable supply. We work with developers, EPC contractors, utilities, system integrators and asset owners across the complete project lifecycle, from early engineering decisions to long-term monitoring and maintenance.

System Design
Installation
Commissioning
Monitoring & Maintenance

Advanced technologies such as EOSS monitoring systems, PRY-CAM diagnostics, Alesea asset management and Smart Drums help improve installation efficiency, support predictive maintenance, increase system availability and protect long-term BESS performance.

Global BESS Expertise with Local Compliance

International experience combined with local energy storage standards and market requirements

With decades of experience in renewable energy, power transmission and grid infrastructure projects worldwide, Prysmian combines global BESS expertise with local execution capabilities.

Whether connecting battery containers, power conversion systems, substations or transmission networks, Prysmian delivers BESS cable and connectivity solutions designed to meet global best practices, national regulations and local compliance requirements.

 

Fit-for-Purpose BESS Solutions for Safer, More Reliable Energy Storage

Technology developed for the practical realities of battery energy storage systems

Battery Energy Storage Systems require dedicated cable, connectivity and monitoring solutions that can support high-power operation, safety-critical environments and future system scalability.

Prysmian’s BESS portfolio is designed around the specific challenges of energy storage applications, including high-power DC circuits, demanding environmental exposure, compact installation layouts, fire safety requirements and long-term asset resilience.

By combining specialized cable technologies, connectivity systems, monitoring solutions and engineering expertise, Prysmian helps customers increase reliability, enhance safety, simplify installation and maximize return on investment in battery energy storage projects.

Because in energy storage, every connection matters.
And every connection starts with the right design.

Project Mufasa, The Netherlands

Reference Case: Project Mufasa, The Netherlands

Supporting one of Europe’s largest battery energy storage systems

Discover more 

BOS Energy Project, Estonia

Reference Case: BOS Energy Project, Estonia

Powering Estonia’s Energy Storage Future

Discover more 

× Project Mufasa, The Netherlands

Reference Case: Project Mufasa, The Netherlands

Supporting one of Europe’s largest battery energy storage systems

Project Mufasa, developed by Return Industrial Solutions, is one of the largest Battery Energy Storage System (BESS) projects in Europe. Located in Vlissingen, in the North Sea Port area of the Netherlands, the project is designed to strengthen grid stability, support renewable energy integration and improve the flexibility of the Dutch power system.

Project Mufasa will deliver large-scale energy storage capacity of approximately 350 MW / 1,400 MWh and is expected to become operational in 2027. The project demonstrates how utility-scale BESS infrastructure can help balance supply and demand, reduce grid congestion and support the transition from fossil-based power generation to renewable electricity.

From power transmission and grid connection to communication, control, fire protection and monitoring systems, projects of this scale require a reliable, integrated infrastructure approach across the full BESS architecture.

By supporting complex energy storage developments such as Mufasa, Prysmian helps enable safer, more resilient and future-ready electricity networks. In BESS projects, every connection plays a critical role.

× BOS Energy Project, Estonia

Reference Case: BOS Energy Project, Estonia

Powering Estonia’s Energy Storage Future

The BOS Energy Project in Paldiski, Estonia, is a major Battery Energy Storage System (BESS) development designed to support grid stability and participate in frequency regulation markets.

The project features a 25 MW / 50 MWh energy storage system and has been developed with battery technology partner Cubenergy. In addition to the BESS installation, a new 110/33 kV customer substation was constructed, together with approximately 1.8 km of 110 kV cable and 4.1 km of new 33 kV underground cable infrastructure.

Connected to the Elering Paldiski 110 kV substation, the project strengthens the local electricity network while creating the potential for future integration of a solar park.