Prysmian teams up for coastal spring clean

Prysmian teams up for coastal spring clean


This Spring the Prysmian team has been out making a splash in East Lothian and County Durham. As part of Prysmian’s commitment to deliver social value on the Eastern Green Link 1 (EGL1) project, the team traded technical gear for litter pickers to support two major environmental campaigns. The multi-billion-pound project is being developed through a joint venture between SP Energy Networks and National Grid Electricity Transmission.

Once complete, EGL1 will play a vital role in strengthening the UK’s electricity network. It will help to transport green, renewable energy efficiently across the country and supporting the transition to a cleaner, more resilient energy system.

Coastal clean in North Berwick

Prysmian's spring cleaning journey began on 10 April at North Berwick in Scotland where two volunteers joined forces with a colleague from supply chain partner, Glenturas.

The event was hosted by the Scottish Seabird Centre as part of Keep Scotland Beautiful’s Spring Clean Scotland campaign. It wasn't just about picking up rubbish; it was about protecting the local marine life and ensuring the beach remains beautiful and safe for the community, and the thousands of seabirds that call it home.

 

Litter pick in Seaham

The momentum continued on 29 April down at Vale Tempest beach in Seaham. This time, the team joined Durham Council for the Great British Spring Clean. It was a true team effort, with three Prysmian volunteers working alongside four colleagues from supply chain partner PBU. Ten bags of litter were cleared from the beach, preventing plastic and debris from washing back into the ocean.

 

The power of volunteering

Across these two events, Prysmian teams recorded a total of 17.5 hours of volunteering, removing over a dozen bags of rubbish.

 

Alberto Pirovano, Project Director at Prysmian said "At Prysmian, we believe that building the energy infrastructure of the future goes hand-in-hand with caring for the communities we work in today. Seeing our teams and supply chain partners come together for the Spring Clean campaigns shows that it’s about more than just cables; it’s about leaving a positive legacy for the environment.

“A huge thank you to everyone who rolled up their sleeves and got stuck in.”

 

These mark the seventh and eighth litter picks the team has undertaken. In 2025, Prysmian worked in close coordination with the Scottish Seabird Centre and Durham Wildlife Trust; participated in six beach cleans, removing dozens of bags of litter to keep the coast clean and safe for everyone to enjoy.

 

 

Additional Information

About Prysmian and EGL1 Social Value

Prysmian is the main contractor for the engineering, procurement, construction, and installation of the HVDC cable system for EGL1. As part of this major infrastructure project, Prysmian is dedicated to delivering significant social value by investing in local communities, supporting local employment and skills, and promoting environmental sustainability throughout the project lifecycle.

 

About Eastern Green Link 1 (EGL1)

EGL1 is a vital national infrastructure project that will see the construction of a new high-voltage direct current (HVDC) electrical cable link between the Torness area in East Lothian, Scotland, and the Hawthorn Pit area in County Durham, England. Developed by National Grid Electricity Transmission and SP Energy Networks (SPEN), the link will play a crucial role in delivering clean energy to homes and businesses across the UK by increasing the nation’s capacity to transport renewable power across the country.