Prysmian to help Germany achieve green energy transition

Prysmian’s innovative cable technology will help Germany achieve sustainable energy transition. Germany plans to install the world’s longest underground cable by 2025 to transmit renewable energy located in its north to its energy-hungry southern regions.

Underground HV cables for the stronger grids of the future

Prysmian Group and other main industry players will take an active role in the energy transition by developing increasingly powerful underground cables needed to cover greater and greater distances, distributing renewable energy throughout the grid as is the case with Germany’s north-south HVDC Corridors plan.

Underground HV cables for the stronger grids of the future

Prysmian Group and other main industry players will take an active role in the energy transition by developing increasingly powerful underground cables needed to cover greater and greater distances, distributing renewable energy throughout the grid as is the case with Germany’s north-south HVDC Corridors plan.

By 2022, Germany will phase out its 17 nuclear power plants, making it even more challenging to achieve its “Energiewende” plan to shift Europe’s industrial powerhouse over to a fossil fuel-free economy by 2050. Despite Germany’s massive investment in renewable energy, the country now faces a major hurdle in achieving its decarbonization goal because its electricity grid is not up to the task of efficiently transporting wind energy generated in the north to where it is needed in the southern regions. 

“As the number of windfarms continues to grow, we will see an increasing need for cables to export and dispatch renewable energy attached to wind farms,” said Borjan Sehovac, High Voltage Business Unit Vice President. Germany’s plan for three major HVDC interconnectors has required Prysmian Group - and other industry players - to develop new solutions like 525 kV underground land cable technology. This higher-voltage cables normally leads to a reduced quantity of cables to transmit the same power (comparing for example 525 kV to a 320 kV DC system), thus requiring less space to install the system, increasing also the overall benefit and efficiency for a project of this size.  Prysmian has launched two new 525 kV cables, one qualified with P-Laser and one with XLPE insulation. P-Laser is the first fully recyclable eco-friendly high-performance cable. Awards for the German HVDC Corridor projects are expected in summer 2020.

The plan is ambitious to say the least, because these underground lines will be the longest in the world and will use a new, higher voltage cables technology. It’s a good example of how Prysmian is stepping up to the plate, explained Borjan Sehovac. “The future will certainly call for more energy dispatchment – stronger grids and safer energy – but for sure with fewer overhead lines. This is the trend of the future market for cables,” said Sehovac. Underground cables are more and more replacing overhead lines, said Sehovac, despite the fact that underground cables cost more up front. They are more eco-friendly and allow for easier permitting because residents and communities are less likely to oppose an underground cable. Underground cables are also safer than overhead lines because they can’t be affected by adverse weather like snow storms or hurricanes, which are becoming increasingly common.

“Less losses, more performance, with a great focus on efficiency, environment and smarter systems. These are the keys for the energy transition.
This is translated into our business in terms of higher voltage levels, bigger cross sections, lower losses, preventive maintenance and recyclable materials.
And this gives really stronger grids.
”

Borjan Sehovac

High Voltage Business Unit Vice President

“Germany will be transmitting clean energy hopefully also using clean connection,” said Sehovac. 
Prysmian is the world’s leading producer of high voltage cables, with a strong leading position in the market and more than 15 HV factories across five continents. It is a global solutions provider, encompassing cable and system design including accessories, and full project management, commissioning and testing, together with maintenance and repair services.
Its global reach is a key success factor, allowing it to share and transfer best practices and inter-company order management between regions, said Sehovac.