DESI examines fixed and mobile broadband supply and demand and progress on the EU’s key digital infrastructure goal: every European household should have access to ‘high-speed’ (100Mbps+) internet coverage by the end of 2025 and gigabit (1000Mbps+) connectivity by the end of 2030. NExsT takes a closer look at the connectivity and broadband aspects of the 2022 report.
Over 188 million EU households (97.9%) had access to at least one of the main fixed broadband access technologies at the end of June 2021. When it comes to fixed broadband take-up, we see that 78% of EU households had a fixed broadband subscription in 2021, following steady growth over the last 9 years. National take-up rates ranged from 61% to 97% with The Netherlands, Cyprus, Luxembourg and Malta registering the highest figures. Coverage of Next Generation Access technologies capable of delivering >30 Mb/s download speeds reached 90.1% of households in 2021, a slight increase of 2.9 percentage points compared to the previous year.
Home internet access is mainly provided through fixed technologies, with stable coverage at 98%. xDSL (digital subscriber line) continued to have the largest footprint (89%) followed by Fixed Wireless Access (FWA) (58%), Fibre to the Premise (FTTP) (50%) and DOCSIS (Data Over Cable Service Interface Specification) 3.0 cable (44%). VDSL (Very high-speed digital subscriber line) coverage remained stable (54.5% of EU households), while cable DOCSIS 3.0 declined slightly. VDSL coverage growth has been decreasing since 2018 as operators have begun to divert investments towards more advanced technologies (especially FTTP) in pursuit of EU Digital Decade targets.