Prysmian is proud to be playing a central role in the development of new strategic infrastructure for UK. Once completed, Eastern Green Link 2 (EGL2) will be the UK’s single biggest ever electricity transmission project, including the longest HVDC cable in the country with approx. 500 km in length and will transport enough clean energy to power around two million homes.