Prysmian has launched the HVDC cable installation for SuedOstLink this October. The joint base is located approx. 270 km from Isar at the northernmost point of the Bavarian SuedOstLink part, to deliver reliable and sustainable power transmission, confirming its strategic role in the shift towards a low-carbon economy and to drive the energy transition forwards with smarter, more reliable, and more sustainable solutions.
The project was awarded to Prysmian by the German grid operator TenneT TSO GmbH with the assignment to deliver a 525 kV HVDC underground cable system with transmittable power of more than 2 GW on a single system. The cables have been produced at the Gron plant (France), one of Prysmian’s center of excellence for underground cables. Prysmian’s subcontractor partners are also part of the project’s execution.