PLATINUM LEED CERTIFIED HQ BUILDING
The 13,200m2 of Prysmian’s HQ offices are an example of contemporary cutting-edge work spaces designed to foster collaboration and agile working. The building consists of three building blocks (wings), which accommodate the offices organised into an open-space arrangement, partitioned by bioclimatic greenhouses that serve for space organisation purposes and natural lighting. The presence of triple-height glazed spaces ensures a direct link between interior and exterior, also accentuated by the numerous green ‘havens’ (greenhouses) and break areas.
The headquarters also boasts a 180-seat auditorium and 100 meeting rooms. Artificial lighting is dynamically controlled according to the ambient brightness values registered by the management system, allowing considerable energy savings compared to a traditional lighting system. On top of this, there are 3,820 m2 plus 2,188 m2 FTV of shelters with photovoltaic panels, 28 electric car charging stations already in place with a further 22 to be added in a very short time for a total of 50 electric car charging stations with double recharge (for 100 cars), two bike parking stations, and 20 stations for separate waste collection.
All this allowed us to obtain the prestigious Platinum LEED certification, demonstrating the efforts made to ensure great attention to the environment even in a highly complex reconversion project. Prysmian’s Headquarters are located in the Bicocca district, in the former Ansaldo industrial area. Today, this part of the city still bears witness to its industrial past, but with a contemporary look, as it is one of the first former industrial areas to undergo a radical transformation. Prysmian’s HQ is an important new chapter for the district, continuing the urban regeneration of a fast-developing part of Milan.